Hi,
I've a question.
In my application I'm using ser DS90UB925Q and des DS90UB926Q, to drive a 640x480@25MHz display true color(24bit) with touchscreen, speed of the link is about 875Mbps. Now I need to switch signals from ser DS90UB925Q to two different des 926Q in two different position, but only one of the two is active.
I just read this topic: http://e2e.ti.com/support/interface/high_speed_interface/f/138/p/209684/745774.aspx#745774
and I understand than FPD-Link III chipsets only support point-to-point applications., no "active" switch or repeater.
But, is possibile with a High-Speed Differential Multiplexer / Demultiplexer like TS3L301 ("with no buffer or repeater inside") or similar to split the signals from SER without interrupt the bidirectional signaling of the FPD-Link III interface?
Thanks
Best regards
Luca