Hi Team,
Please advise me answering to the questions bellows.
I appreciate it if you can give us prompt feedback, because we are
now testing EVK and need to make it works ASAP.
Q1. The default value of the DE control register (0x11 or others) is 0x03.
In the meantime, there is no description of the value 0x03 for the DE control register.
Is 0x03 is typo?
If so, what is the default value for DE control?
If it is correct value, what DE effect, does DS64BR401 shows?
00 = 00000001 = 01'h = 0.0 dB
01 = 00111000 = 38'h = −3.5 dB
0F = 10001000 = 88'h = −6.0 dB
01 = 10010000 = 90'h = −9.0 dB
1F = 10100000 = A0'h = −12.0 dB
F0 = 10010000 = 90'h = −9.0 dB
F1 = 10100000 = A0'h = −12.0 dB
FF = 11000000 = C0'h = Reserved
Q2. IDEL RATE select register (0x0E or others) specifies the rate 2.5-3Gbps or 5-6Gbps.
Doesn’t the chip support 1.5Gbps SATA?
When you need to support 1.5Gbps SATA, how do you set up this register?
Q3. Auto rate mode is not the default value of IDEL RATE select register (0x0E)
Why the Auto Rate mode is not selected as the default?
Q4. Can DS64BR401 be used in SATA application when it is configured in SM-Bus
mode and registers are set in default value?
Are there any registers to be changed when it is sued in SATA application, (except
EQ and DE optimizing)
If here are some registers to be changed, can you provide us the saved configuration file for ALP software.
Mita