Hello,
I have questions about GPO of DS90UB913A-Q1.
(1) GPO Direction bits of Control Registers
In the datasheet P.29, GPO0~3 direction can be configured input or output.
However I think that these GPOs can not be configured to input or output.
Could you please let me know the meaning of GPO direction bits?
(3)GPO2 output freaquency at the External Oscillator Mode
Please see the attached file.
6675.20140902_GPO DS90UB913.pdf
If I use DS90UB913A as external oscillator mode 10bit mode, GPO2 output clock is double of GPO3 input clock.
(i.e, If GPO3 input is 48MHz, GPO2 output is 96MHz)
Is my understanding correct?
I would like to confirm this due to there is "÷2" in the figure 26 of datasheet P.42.
Best Regards,
Ryuji Asaka