Hi all,
Would you mind if we ask TS3DV642?
Our customer wants to switch 3G-SDI(HD/SD) signals from SPF+ or LMH0387 using TS3DV642.
(Please refer to attachmentfile.)
5280.0361.5025.Construction.pdf
On this construction, according to using TS3DV642, we have following questions.
<Question>
1. Is it possible to construct the system like as attachmentfile?
2. And then, if it is possible, what should we notice?(Jitter, some effect)
3. Location of AC-coupling capacitance
-We found on the data sheet that it recommends that AC-coupling capacitance should be placed at output side(D0 +/-).
On the our customer case, does it say the same?
Please let know us these.
Kind regards,
Hirotaka Matsumoto