Hi team,
Please advise me on the following questions.
Q1. On page 59, Figure 46 shows the allowable loss curves and EQ gain curve.
Can you explain why allowable loss curve of the STP is 3 dB higher than those Coax?
Why the allowable loss is 3/6 dB higher than EQ curve?
Q2. Do you know any smaller size coil than L3/L1 (COILCRAFT_KA4909-NO-STUFF) on the EVKs(
DS90UB913A-CXEVM & DS90UB914A-CXEVM). (Smaller than WxLxH 5x5x3 mm)
When you chose alternative coil, can you let me know the characteristics you need to focus?
Q3. When you use a STP cable to transfer power and signal, can you transfer power using only
differential pair instead of Differential pair and Shield?
(The DC 12V is connected to DOUT+ and return power is connected to DOUT-)
If it is feasible, can you provide me a reference schematic to implement such configuration?
Mita