Hi,
I am using the DS90UB914Q Demo board rev A connected to a Freescale iMX6 board.
The I2C bus of the iMX6 is connected to the I2C bus of the demo board but the bus operation is stopped since the DS90UB914Q always keep the SCL to low.
In such situation the I2C driver running on the iMX6 processor detects "Connection timeout" every time it is reading from the I2C bus.
I am wondering if the I2C slave is burned out on the chip or if there is something wrong I am doing.
Dip switches configuration is OK. Leds on the board are ON so it is alive.
Pull up resistors are properly set.
Thank you in advance
Andrea