We have a design utilizing the DS90C387A to transmit parallel 24-bit video to an LCD panel in single-to-dual pixel conversion at an input clock rate of 148.8MHz for an effective LVDS clock rate of 74.4MHz. Pre-emphasis is set to 100%.
We are connecting the board using the DS90C387A to the display with a micro-coax 100Ohm cable. At cable lengths less than 9-inches, things work great and the video is crisp. Using a 4-foot cable, black bars appear which get progressively larger the further into the frame the video gets. Using a 9-foot cable produces a black screen with an occasional short lived flicker.
The data sheet for the DS90C387 states that for an LVDS clock rate of 65MHz, a cable length of 10 meters can be used and for a clock rate of 80MHz, a cable of 7 meters can be used with 30% pre-emphasis and a cable of 2 meters can be used with 25% pre-emphasis. Note 19 in the data sheet states that a shielded twisted pair cable was used. Can anybody provide any further information on this test setup? What the gauge of the cable is and how much error is acceptable in these tests? Also, there is no test data for setting the pre-emphasis higher than 50%. What is the consequence of a higher pre-emphasis? Is there a reason that I am unable to achieve success with a 4-foot cable?