This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum Junction Temperatures and Rjc

Other Parts Discussed in Thread: DS26LV32AQML

I'm looking for the maximum junction temperatures and junction-to-case thermal resistances for the following components.  Any and all help would be greatly appreciated.

5962-9762101QFA

5962-9762201QFA

SN65LVDS31D

DS26LV32AQML

  • Hi Jared,

    This will take a bit of time because we will need to put in a request from our thermal modeling team. I will get back in a week's time to see what we can do.

    Thanks,

    Michael

  • Hi Jared,

    So far, the only data I am able to retrieve are the thermals for the SN65LVDS31D. See below:

    Theta_JA 84.8
    Theta_JC (top) 46
    Theta_JB 41.8
    Psi_JT 11.1
    Psi_JB 41.5
    Theta_JC (bottom) n/a

    Hope this helps!

    Michael

  • Hi Jared,

    I have recently attained data for the DS26LV32A, in C/W.

    Theta_JA 109.5 (for reference only)
    Theta_JC (top) N/A
    Theta_JB 97.5 (for reference only)
    Psi_JT 28.2
    Psi_JB N/A
    Theta_JC (bottom) 6.2

    From our packaging team: 

    "The DS26LV32A is sold as an unformed part, so actual Theta_JA, Theta_JB depends on lead form. Usually this part type will be used with package underfill and/or conformal cost which JESD 51 does not encompass as well, so these values are for reference only".

    So far, the request for the remaining parts in your original post have not been closed, and I do not have an estimate about their completion date.

    I hope that the thermals we have been able to provide will serve as a good guideline about typical thermal values to expect.

    Thanks,

    Michael