Hi Team,
The output pin of DS34RT5110 and the HDMI Connector pin assign is in the opposite direction. In this case you would need to use via and place the HDMI connector on the opposite side of the board.
[Question]
Why was the pin assign designed this way ? I believe it is difficult to keep 50ohm impedance at the via which would cause reflection. Does the device have enough characteristic using the via in the trace between device and the connector, like the EVM ?
[Question]
Our customer will place common mode choke coil (CMCC) to lower EMI.
Do you have a recommendation where you should place the CMCC ?
DS34RT5110--[]------------[]--VIA--[]------------[]--HDMI Connector
A B C D
Should you place close to the device output pins, such as point A above ?
Best Regards,
Kawai