Hi,
I would like to confirm a frequency variation for Free-run control voltage.
If we change VC_Free[9:0] register for each step, is the frequency variation the following formula ?
Frequency variation[Hz] = 3.3V / 2^10 * Kv , where 3.3V is VCC and Kv is the tunig sensitivity of the VCXO in use.
For example, a system with Kv = 1000Hz/V, will have a frequency variation of 3.2mV *1000 = 3.2Hz. Is my understanding correct?
Best Regards,
Kato