Hi,
I'm considering use of DS90UB926 for output of a TFT display.
But, I'd like to reduce the number of bits of the output, so it prefers to output by RGB565 format.
I read a datasheet, there was no mentioning about RGB565, and I didn't know whether it could be used.
It outputs by the format of RGB666, and is it possible to use as RGB565 format by using only upper 5bit of output of B and R?
Would I be able to achieve RGB565 format output by an upper way?
But, I don't know whether serializer input is RGB666 or RGB565.
When it can't correspond to RGB565 easily, it'll be used in RGB666.
thanks.