Hi,
The DS15EA101 equalizer says within the datasheet that it does not support transformer coupling. If transformer coupling is required for my application is there a method by which this device can be made to work? It meets all of the other needs i currently have including the industrial range. My application is a 1.2Gbps 8b/10b encoded data stream over a cable that can range in length from 1m to 25m. If I add pull up resistors and AC coupling caps from the output of the transformer, does the equalizer device support that method of input? Or even a termination impedance with AC coupling caps between the output of the transformer and the input of the DS15EA101?
If the DS15EA101 will not work in my application at all due to my need for transformer coupling, is there another industrial grade adaptive equalizer that will function for me?
Thanks
Marty