Hello,
I'm looking for sn55lvds32 and sn55lvds31 ibis model. As there is none available, does anybody know if I can use sn65lvds32 and sn65lvds31 instead?
If yes, anything special I need to care of ?
Thanks,
Luca
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm looking for sn55lvds32 and sn55lvds31 ibis model. As there is none available, does anybody know if I can use sn65lvds32 and sn65lvds31 instead?
If yes, anything special I need to care of ?
Thanks,
Luca
Wade, I can't see this post.
Following error appear.
You do not have permission to view/download this item.
Regards,
Luca
Sorry Luca. I did not realize that was an internal post.
Here are the models. Note, I included the LVDS31 LVDS32, and LVDS33 in W package for completeness.
Note, they are the same as the commercial models, with modified parasitics for the different package.
Regards,
Wade