Dear Sir
I would like to use DS90UB929 and DS90UB940 for HDMI to MIPI Panel
I have some question
1. DS90UB940 can't be a master mode to read SPI Flash or EEPROM register automaticly ,Is it right? ( 940's SPI or I2C will pass the signal from host side or device side)
2.If I want to use one pin of DS90UB940 to controller "MIPI Mux 2:1 switch" channel selection when HDMI cable insert in DS90UB929 (PS. DS90UB940 detect some of signal deliver from DS90UB929)
How could I do this function??
Thanks