I have a customer who wants to connect mulitple signage tiles using 2' lengths of CAT6 cable using LVDS deserializers on each tile and then driving the LVDS signal to the next tile using a cable driver. The customer has the following questions:
I'd like some advice on how to connect each LVDS receiver to LVDS Deserializer and LVDS cable driver on each tile.
If I use DS15EA101 as receiver, its output feeds into DS15BA101 and into SN65LVDS1224.
Since it is a 10bit system, documentation suggest for a DC coupled connection.
From DS15EA101 I run 2 wires straight into 1224 and I add a 100 ohm parallel resistor for line impedance.
Can these 2 wires go straight into DS15BA101 to reamplify the line ? Do they need AC coupled ?
What are the issues related to having 2 inputs (1224 and BA101) behind one output (EA101) ? Any schematic suggestion from TI ?
LVDS speed is in the 400Mbps range.