Hi Expert,
Could you please show us internal pulldown value of PDB ?
According to datasheet, I guess min Pulldown value can be caluculated as shown below.
* Max input current is 10uA and min VDDIO is 3.3*0.9 = 2.97V
So, min pulldown value is
2.97 / (10 * 10^-6) = 300k ohm
(But I'm not sure whether 10uA is value in case of internal pulldown was enabled or not..)
Is my understanding correct ?
Best Regards,
Machida