Hello,
In DS90UR241/124 datasheet page 30, there is the discription of the "External bypass capacitors should include both RF ceramic and tantalum electrolytic types".
(1) Tanatalum electrolytic cap
Can I use ceramic capacitors instead of tantalum electrolytic types?
Since the datashee was published on 2006, I think that the datasheet use tantalum type because the ceramic capacitors DC rating was small on 2006.
However, the ceramic capacitors DC voltage rating is increased by technologyadvance.
Thus , we can choose the ceramic capacitors which has the range of 2.2uF to 10uF with 5xPower supply voltage rating.
(2)Typical application connection
I can't found the 2.2uF to 10uF capacitors in the typical application connection Figure 22 and 26.
Please let me know this reason.
(3) User's guide schematics
In the SERDESUR-43USB User's guide page 25, there is the bypass capacitors combination as 0.01uF and 0.1uF and 22uF.
Why does this schematic use 22uF as a bypass capacitor?
The datasheet recommendation capacitor range is 2.2uF to 10uF.
Best Regards,
Ryuji Asaka