Hi,
I would like to ask you some questions about DS80PCI800 as below.
Now I am planning to make following system.
TX : CPU =(max length 8inch)=> ”DS80PCI800” =(max length 0.4 inch)=> PCI-Slot/Card
RX: CPU <=(max length 4inch)= ”DS80PCI800” <=(max length 8.4inch)= PCI-Slot/Card
I assume that PCIE cards are Gen2 and Gen3 certificated.
Q1) Pin-Mode
In case of using DS80PC800 as “Pin-Mode”, following settings are correct?
ENSMB |
GND |
Pin Mode |
VDD_SEL |
GND |
3.3-V mode |
RATE |
FLOAT |
AUTO Rate Select of Gen1/2 and Gen3 with de-emphasis |
RXDET |
FLOAT |
|
SD_TH |
FLOAT |
ASSERT LEVEL is 180 mVp-p |
PRSNT |
1K-GND |
Q2) Equalizer Setting
Q2-1) trace length
I think that the setting of EQ level will be determined by checking the real signal quality finally.
Is this correct? On the other hand, in case of “circuit design” phase, how should we set EQ?
We can set EQ according to “real trace length”, right?
Q2-2) Data sheet “Table 2”
There is a “Suggested use” column in Table 2. There describes the “Trace length”
Does this length include “internal trace length of the card which is inserted to connector” or not?
Just the length from PCIE slot pin to “ReDriver” pin, correct?
Q3) Emphasis setting
About the following note(1) of Table 3,
“The de-emphasis levels are available in GEN1, GEN2, and GEN 3 modes when RATE = Float.”
Can I understand this note that we should set “RATE” pin as “Float(Auto)” to activate the level
setting of De-Emphasis? Or the level setting will be also activated by the setting of “1K-GND(Gen1/2)”
or “1K-VDD(Gen3 with Emphasis)”?
Q4) Suggested level setting
There is a description about the trace length of RX side on “9.1.2” section.
About the sentence I underlined “Red”, my understanding is,
“We should set the level of Gen3 corresponding to Gen3 trace length under the condition of
“trace length of RX side is “< 5 Inch” and TX side is “5 inch 4-mil””.
Is this correct?
Q5)Confirmation of EQ/DEM level setting (Again)
As of now, I have understood followings.
Circuit design phase --- to set the level by the real trace length
Final (like pre-production) phase --- tuning by checking “Eye pattern”
Is this correct?
Thank you for your support.
Best Regards,