I'm developing boundary scan test for our scanner product and now focusing to backplane connector. My idea is to do adapter board were SCAN15MB200 LVDS buffer outputs are connected via backplane connector to the LVDS receiver in the baseboard. There are both AC-coupled and DC-coupled signals in the backplane connector.
Can I leave buffer input pins floating when output is connected? And can I left other unused LVDS IO’s floating? Boundary scan tool is using IO’s in 10MHz clock frequency. For boundary scan testing I don’t have need for high speed signalling.
I could not find SCAN15MB200 BSDL file from the webpage. Is it available somewhere?