Hello,
is it possible to use the TLK2711A at a datarate only 1 GBPS? We need the special KWORD features of this chip so we can't use the TLK1501.
Regards,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
is it possible to use the TLK2711A at a datarate only 1 GBPS? We need the special KWORD features of this chip so we can't use the TLK1501.
Regards,
Michael
Hi Michael,
TLK2711A does not support 1Gbps datarate, but you could take a look into another devices such as:
TLK2541 ==> 1 to 2.6Gbps Transceiver (K-coding)
TLK2208 ==> 1 to 1.3Gbps Transceiver (K-coding)
Best Regards,
Luis Omar Morán Serna
High Speed Interface
SWAT Team
Hi Luis,
thank you for the quick response. I will take a look at the suggested devices.
Best Regards
Michael