I need to know if the SN75LVCP601 SATA re-driver will drive a 2 meter eSATA cable at SATA II (3 Gbps) speeds, or if I need to use a different re-driver.
I am currently using it for SATA interfaces that are within a backplane/chassis, therefore, no external cables, just PCB traces and connectors. Now, we want to take some of these interfaces and make them external, with up to a 2-meter eSATA cable.
We'd prefer to keep the same part, but are not against introducing a new chip to get the 2-meter cable driving performance we need. The amount of FR4 trace the signal would have to go through before hitting the connector is about 12-18 inches. There is one picture in the SN75LVCP601 datasheet that implies that the re-driver can drive a 2m cable, but there is nothing else in the spec that specifically mentions it.
The TI E2E community mentions alternate parts, such as:
SN75LVCP412
SN75LVCP412A
DS100BR111
DS64BR111
DS100BR410
SN75LVPE802
The SN75LVCP412 specifically says "eSATA compliant" and "data rates up to 3.0 Gbps". It sounds like this one might be good, because it doesn't work above 3 Gbps so perhaps the tradeoff is that it can drive a longer cable. Any suggestions as to re-drivers that work up to 3 Gbps and can drive a 2-meter cable would be appreciated.
Thanks!