Hi everyone,
I am new in this forum, and maybe what I am asking is obvious.So firstly my apologizes.
I want to try to do a 4X1 HD-SDI switch. For this I have the LMH0376 4x1 reclocker. I know this device is intended to work with cable equalizer on the inputs and also a cable driver on output. The input is a 100ohm differential input. My application will use a really short coax cable, in the inputs and output. Could I use this 100ohm differential input as a 75ohm single-end input? and also the same with the output? I need a really small PCB, and as the cables length will be really short I though to avoid the Equalizers and drivers..
maybe is an stupid question, but I am not an electronic engineer and I will appreciate any answer or advice.
thanks in advance,
Jordi