This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Madhu,
SMPTE Specifies jitter - in the form of timing and aliment jitter - at the output of the transmitter. However, i am not aware of a jitter spec at the output of the equalizer. SMPTE specifies parameters on the 75 ohm SDI side but not on the 100 ohm differential side. Having said this, please below note responses to your questions:
1). Yes these are maximum total jitter(there is no filter to limit the jitter).
2). Under the condition specified in the data sheet, this is the maximum jitter. However, if conditions noted in the data sheet are violated - for example the source transmitter has high jitter or longer cable length are used - then there maybe higher output jitter. I say maybe since this condition has not been characterized or evaluated.
3). Could you please send us a block diagram of your project so we can get a good overview of your application? This would enable us to better answer your questions.
Regards,,nasser
Hi,
Please find the SDI receiver block diagram below. Since the cable length will be more and there is a possibility of jitter, I have included a reclocker between FPGA and Equalizer. Please let me know whether the reclocker position ( between equalizer and fpga) is proper for eliminating jitter. Also please let me know if there is any other reclocker for SDI with better characteristics.
Regards
Madhu Sharma
Hi Michael,
The second case you mentioned: 2. Before a Cable Driver device and after the FPGA or Cable EQ
What is the advantage of connecting th Reclocker between Cable driver and FPGA??
Regards
Madhu
Hi Michael,
In my application, the SDI camera will be far away from the board where equalizer is present. And, the FPGA will be very near to SDI driver. So I'm using reclocker only between equalizer and the FPGA.
For the reclocker LMH0346MH/NOPB,
1)If the second output pins are not used, how to connect SCO/SDO2, its inverse signal and SCO_EN pins?
2) Any design guidelines ( such as decoupling, layout recommendation etc) available for this device?
3) Whether both VCCO and VCC can be connected to single 3.3V supply?
Regards
Madhu