This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVP20 Input Termination

Other Parts Discussed in Thread: SN65LVP20

I would like to use the SN65LVP20 device in a new design.

A couple of quick questions on input termination for the SN65LVP20:

1) Does the SN65LVP20 have internal termination on its inputs or is external termination required?

The .pdf does not state & there are not any examples.

2) If the SN65LVP20 has internal termination, is this common to other "LVP" devices (ex. CDCLVP1210, CDCLVP1024).

I need to use all 3 devices and want to make sure the termination is correct as I am ready to move forward to layout.

Also, any examples that show input / output termination would be helpful.

Thanks in advance,
- Michael Lawson