Hi,
Is there a reference diagram of the AC-coupled interface to the differential receiver?
Best regards,
Seishin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Seishin-san,
You can refer to the following app note as a reference: http://www.ti.com/lit/an/scaa059c/scaa059c.pdf
If you are interfacing to an LVDS or CML receiver, it is important to determine whether the receiver is self-biased. It seems from your diagram that there is an internal termination to a CML receiver, so I recommend looking at Figure 13 in the app note. Also ensure since you are using AC coupling that the data you are sending through is DC-balanced.
Thanks,
Michael