In LMH0324-18EVM_SNLU182.pdf (LMH0324 Evaluation Module User's Guide), a return loss network (3.3nH inductor in parallel with a 75 ohm resistor) is in on the output, OUT0+/- (pins 20 & 19) of the LMH0318. However, it is not on the other output, OUT1+/-. Why is a return loss network on one output but not the other?
Also, there is no mention of the return loss network in the LMH0318 datasheet. It is not shown in the sample configuration drawing either.
Furthermore, the return loss network is not on OUT0+/- of LMH1218 on the LMH1218EVM (snlu173a).
Is the return loss network needed for the LMH0318? If so, why is it needed for OUT0 but not OUT1 on the LMH0318 but not the LMH1218, which is footprint compatible.
Thanks!
Mark