Good evening,
I need your help with the DS80PCI800 PCIe redriver which I want to configure with an external EEPROM.
The PCIe redriver works fine and each DS80PCI800 read his configuration from the installed EEPROM but I have one problem with the PCIe Generation configuration. The hardware RATE pin is floating, this mean that the redriver set the PCIe Generation by his own. In the EEPROM configuration I found one bit which is called OVRD_RATE, this bit is set to 0 (Allow RATE Pin control) but the redriver use the EEPROM PCIe generation settings for each channel.
If I connect a Gen 1 or 2 PCIe card to the redriver and I configured the RATE_sel for a Gen 3 card, the PCIe card don't work correct. If I re-configur the EEPROM data for Gen 1/2 the PCIe card works fine.
I don't know why the hardware RATE pin has no impact for the redriver.
Can you help me in this matter?
It's not so customer friendly to re-configure the EEPROM for each slot and PCIe card.
It would be better to use the RATE pin as discribed in the datasheet.
I hope anyone can help me.
Have a nice weekend.
Best regards,
Christian Bräuninger