Part Number: TLK6002EVM
I have the TLK6002EVM and MDIO EVM boards connected and powered. I am using the Sonic MDIO Software to configure and communicate with the two boards. When I use Clause 22 READs of registers 0x00, I receive an "err" return. I am booting the board and then trying to read the registers, so I believe I should receive the default value "0600".
Is there something else I need to do?
example
START
CLAUSE 22
READ(0000)
STOP
When, using Clause 45 READs of the 8000 registers, I receive "FFFF" as expected.
Thank you,
JT