I have a system with two ASICs communicating one-way (simplex) using 400 MHz LVDs signalling. I need to test what happens to the receiver ASIC when the LVDS signals are interrupted (the three test cases are disconnected, shorted to ground, and shorted to VCC). Could I use a SN65LVDS125A (or similar Crosspoint switch) in my test setup?
My thought is to have the LVDS data from the transmitting ASIC connected to 1A and 1B, ground 2A and 2B, tie 3A and 3C to VCC, and leave 4A and 4B floating. I would have 1Y and 1Z connected to my receiving ASIC. Then, depending on the input to the select lines, I can simulate an LVDS interruption in my system.
Any thoughts? Are there any outright reasons this won't work?
Thanks.