Hi,
We are using TI’s TLK10031 10G Ethernet Transceiver as a phy-layer chip to interface an FPGA XAUI port. I am stuck at its MDIO port. There is no response when read it. It looks like floating (all "1”s). I have checked the chip's reset pin (H5) as well as channel power down pin(A8). They are all logic high(=1.8V). The MDIO waveform meets the MDIO-C45 standard with MDC of 5MHz . The port has a pull up resistor of 2K. ST pin(M9) is pull down to ground via a 10K resistor. All power supply voltages look right (within 5%).
Do you have any suggestion for it?
Appreciate a lot!