Hello,
My customer has a question about input equalizer characteristics of SN75LVCP601.
I do not have an evaluation board and measurement environment.
Please answer the question from me.
Data sheet of SN76LVCP601 Conditions in Figure 11 and Figure 12 on page 12:
Case 1 at 6 Gbps
EQ = 14 dB
DE = –2 dB
TP2 Eye Amplitude 240mV (Figure 11. Test Point 2)
TP3 Eye Amplitude 788.8mV (Figure 12. Test Point 3)
Question :
When the above conditions is changed to EQ = 0dB and DE = 0dB, How is the voltage value at TP3?
I believe that the same voltage as the 240mV of TP2 will be outputted in my expectation.
Best Regards,
Hiroaki Masumoto