dear Sir
When we connect 2m cable with 964 ,the screen will have blink ,but if we change to use 10m cable ,the screen will not have blink
do you have any suggest about this issue ??
below is 2m and 10m register value
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear Sir
When we connect 2m cable with 964 ,the screen will have blink ,but if we change to use 10m cable ,the screen will not have blink
do you have any suggest about this issue ??
below is 2m and 10m register value
Thanks
Kai,
sorry I can't open the attached. could you please help paste the plot here?
regarding your issue, please help check:
1. Please read AEQ registers 0xD2–0xD5 when working at 2m and 10m respectively;
2. The 2m and 10m cable are from same vendor? which vendor? please past the S21/S12 parameters here. thanks.
best regards,
Steven
dear Junqiang
1. Register compare as below
2. Register 0x22 / 0x37 / 0x4D / 0x4E / 0x56 / 0xDB is different ,but all of register are read only
3. Both of 2M and 10M cable AEQ register
0xD2 = 84
0xD3 = 27
0xD4 = 60
0xD5 = F8
1. do you have any idea about 2M cable screen blinking issue
2. 0xD5 bit 3:0 have description reg_35[5:4] ,but I can't find this register and don't understand what means Adaptive EQ floor value
3.0xD2 in our setting is 84 ,so bit2 is 1 ,May I know what's different between 1 and 0 ?? due to default value is 0