Other Parts Discussed in Thread: DS90LV001, , DS25BR110
I need to connect two board with LVDS signal. The distance between these two boads is 6 meters. I want two use DS90LV001 as the buffer on the receiver board. But I am worried that one buffer is not enough. So I want to add DS90LV004 on the transmit boad. Is it OK? Or is there any better suggestions?