Hi TI,
my custoer wan to use a free register in DS90UB914A.
The free address means read/write register address/bit and it has not no effect of the device function.
My customer told me that they are using address 0x18 of DS90UB926 as a free register.
(I'm not sure it is TI's recommendation, or not.)
Well, if a free register bit is available on DS90UB914A and DS90UB934,
please let me know the address and bit ? ( only 1bit is enough at this time)