Other Parts Discussed in Thread: USB2ANY, ALP
Hi, team. I have troubles when using the Analog launchpad with the DS90UB949-Q1EVM board,
The information that I need to get is related to the HDMI, but that is the one tab that does not appear (see image below). How can I get the HDMI tab to appear?
In my setup I had the laptop connected to the board via HDMI and I was duplicating the image. The only messages that I found in the MainGui.log are:
(<class exceptions.AttributeError at 0x00254990>, <exceptions.AttributeError instance at 0x034C32D8>, <traceback object at 0x034C3328>)
SerialNum: 0C381B5120001C00
Opening USB2ANY... Obtained handle for 0C381B5120001C00 as 12304
True
DS90UB949
(<class exceptions.AttributeError at 0x00254990>, <exceptions.AttributeError instance at 0x034C3A30>, <traceback object at 0x0565B288>)
SerialNum: 0C381B5120001C00
Opening USB2ANY... Obtained handle for 0C381B5120001C00 as 12304