Hi,
we use your products DS90UB928 and DS90UB927 in interactive driver terminals in public transportation.
As we try to use new display with higher resolution, we have faced frequent, short and random problems with lost synchronisation at deserializer side (which produce graphic errors).
Details of our design:
- FPD link III connection via 10m STP Cat.6 cable
- Last stable graphic configuration: 1024x600/18
- Current unstable graphic configuration: 1280x800/18
At that unstable resolution 1280x800/18 is LVDS clock at aprox. 71 MHz (no spread spectrum activated). There is stated maximum LVDS clock frequency 85 MHz in the datasheet that leads to decision that it should be working.
At what highest resolution do you achieve a steady picture when using a 10m STP Cat.6 cable?