Hi,
i am a bit confused about differences between synchronouos to non-synchronous mode at 953 & 954, and some other MISC question.
can you please elaborate on differences between synchronouos to non-synchronouos mode (limitations are not clearly mentioned in datasheet):
1. which modes (synchronouos vs. non synchronous) are supported for COAX (some changes has been implemented between preliminary to non preliminary data-sheets)?
2. how does these differences impacts integration, please refer to the following topics:
3. reference clock for FPD channel, is it relevant for system developement or it should be transparent for external user?
4. 954 CSI output frequency? I understand that any of the modes impacts MIPI-CSI frequency.
5. Is there an integration limitation that requires MIPI CSI Rx received by 953 to be synchronized to CLK_OUT pin generated by 953?
6. can you please specificly elaborate differences between synchronuous to non-synchronouos mode? according to datasheet it is mentioned that re-synchronization & extra buffering is required for non-synchronuous mode --> where & why extra buffering & re-synchronization are required for non-synchronuous mode?
7. why there is a reigster for configuration of continuous mode both at 953 & 954? as i see it configuration of 954 for continuous node is enough? where am i wrong in my assumption?
8. Which mode is required to be configured by 954 in order to support 913? Is it raw mode?