This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK2711

Other Parts Discussed in Thread: TLK2501, TLK2711-SP

1. I hope to recommend the replacement chip of pin to pin of TLK2711AIRCP.


2. Is TLK2501 an alternative to TLK2711AIRCP?

  • Hi Eric,

    Unfortunately we do not have a direct replacement, although there is the SP version (TLK2711-SP) that is active. On the other hand, the TLK2501 is the closest “replacement”, basically both devices share the same functionality, but the transmitter/receiver electrical characteristics differs a little bit (not critical).

    On the other hand, both devices are not pin to pin compatible, are pretty similar but not equal.

     

    Best Regards,

    Luis Omar Moran

    High Speed Interface

    SWAT Team

  • Hello Eric,

    The TLK2501 could be used as a replacement for the TLK2711A. Please look at the datasheets for the differences to make sure TLK2501 will work for your application. One of the differences to be aware of is that TLK2501 requires external resistors on RX inputs, while TLK2711 RX inputs have built-in termination resistors.

    Regards,
    Yaser