Dear TI,
At the DS90UB934-Q1EVM user guide page 21, there is a PCB schematic of this EVM.
And it seems that pin 43 is a input pin for MIPI_SEL, and pin 12/11, 19/18, 14/13, 16/15, 22/21, 24/23 support the CSI output interface.
However, at the datasheet of DS90UB934-Q1, the pin 43 is reserved, and must be NC or tied to GND for normal operation.
Which one is right?
Does UB934 support MIPI output or not?
thanks,
TS