DS90UB913A-Q1: Which is the default mode either 10-bit or 12-bit?

Part Number: DS90UB913A-Q1

[ DS90UB913A-Q1 ] Which is the default mode either 10-bit or 12-bit?

Hi,

Which is the default mode of DS90UB913A-Q1 either 10-bit or 12-bit after power-up?

I know the mode 10-bit or 12-bit of DS90UB913A-Q1 is set by DS90UB914A-Q1 through back-channel. And, from the 0x05 register of DS90UB9i13A-Q1, it seems that both modes are NOT selected. Please help to make sure the default mode just after power-up.





Thanks,
Ken


<Related Post>:

DS90UB914A-Q1: MODE Settling Time
e2e.ti.com/.../2540410

1 Reply