Hi,
Lot of discussion about DS100DF410SQE to work with 1GbE mode.
As per datasheet we need set only these two registers need to be set for 1GbE application,
For 1GbE applications, it is required to bypass the CDR by setting the override bit 5 of register 0x09 to 1, and set
the data mux bits [7:5] to 3'b000 of register 0x1E.
Other than these two registers any other registers need to set for 1GbE ?