This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

PCA9306: Swapping SCL & SDA

Part Number: PCA9306

Hello,

As far as I can tell, the circuits for SCL and SDA channels appear to be identical.  I want to swap the lines for layout reasons, but I'm worried I will encounter some problem.

So, for example, current layout is:

MASTER_SDA <=> SDA1 - SDA2 <=> SLAVE_SDA

MASTER_SCL => SCL1  - SCL2 => SLAVE_SCL

I want to change to:

MASTER_SDA <=> SCL1 - SCL2 <=> SLAVE_SDA

MASTER_SCL => SDA1 - SDA2 => SLAVE_SCL

This shouldn't cause any problems for I2C @ 400kHz translating from 1.8V to 3.3V, correct?

  • Hello Mark,
    The circuit is identical for each SDA and SCL. You are good to go swapping.
    -Francis Houde
  • In reply to fhoude:

    Great, I thought so but I had to check.

    Thank you

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.