This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

PCA9515B: VOH Specification

Part Number: PCA9515B

Hello

            On datasheet, it has VOL specification as below but no VOH Specification. What is VOH specification of PCA9515B? Thank you.  

BR

Patrick

  • Hi Patrick,

    I2C is an open-drain interface, which means that devices drive a low level but high levels are undriven (and pulled up externally via resistors). So, the high-level output voltage will depend on the pull-up voltage that is used. It will be very close to the pull-up voltage, but there may be some small voltage drop across the pull-up resistor due to leakage currents. (The input current to PCA9515B in the high state is only about 1 uA, though.)

    Max
  • Hey Patrick,

    There is no such thing as VoH in I2C because the transceivers are not capable of driving a signal high. The high signal comes from the pull up resistor and NOT the transceiver.

    -Bobby

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.