Hello,
I have been looking at the TCA9544A, We have four slave devices we plan to connect, Three of the devices are have Interrupt pins but our fourth device which is an OLED Display does not have an interrupt. Would the OLED display still work with TCA9544A and would we tie the fourth I2C slave interrupt to ground?
Also my other question would be three of my slave devices require to be tied up to 3.6V and one slave device require 5V for tie up.
My Question is can I connect all these slaves to my master which requires a pull up of 1.8V using the TCA9544A?
On the datasheet description (first page) is says:
'This allows the use of different bus voltages on each pair, so that 1.8-V, 2.5-V, or 3.3-V parts can communicate with 5-V parts without any additional protection'
Which confused me.
Best regards Mohammed Al-Amin