Hello,
I have a TCA8418 on my design with Vcc=1.8V. Any time I press a key, other ones are detected.
On each column and each row i have a CEM filters with 2x47pF. When a key is pressed, there are 4*47pF charged by the internal 100kohm pull-up.
I measured a 300µs periodic 0V pulse. Due to those capacitors, when the pulse goes from 0 to Vcc, the edge is "good" but not perfect: 10µs between 0V and Vihmin (=1.8*0.7).
Everything works when I completely remove those filters.
I concluded that the problem are the capacitors.
So my question is : what is the maximum capacitor that the TCA8418 can receive on its inputs ?
Or, say differently, what is the maximum acceptable delay between the rising edge of the pulse and Vihmin ?
NB: I can't add external pull-up.