Hi Team,
Customer uses PCA9546A and met some issues.
Could you help for the questions:
1. If the customer use I2C read, then I2C cannot write successfully. Please provide your comment for this behavior is expected or not?
2. how to know the internal Channel status( open or connect)?
Here two experiment that customer test.
1. write fail case:
step 1: set low on reset pin to reset chip.
step 2 :control Channel 1~4 sequencing.( the master will use I2C to read channel status, if the channel is not connect, customer will use I2C write to set channel to connect.) However, the I2C write is fail.
step 3 : customer use I2C write to write 0 value to turn off all channel. However, it is fail.
2. write success case
step 1: set low on reset pin to reset chip.
step 2 :control Channel 1~4 sequencing.( the master will not use I2C to read channel status. The I2C write is successful.
step 3 : customer use I2C write to write 0 value to turn off all channel. I2C wite is successful. But customer would like to know how to make sure the channel turn off or not.
Thanks,
SHH