What is the relationship between switching frequency and current consumption on Vcca and Vccb? Device will be operated with Vcca = 1.8V and Vccb = 3.3V at 80KHz. Need to know the maximum ICC on both rails under these conditions.
Also, what is the difference between the TCA9517 and the TCA9517A? I can't find anything in the datasheets.