If there relation graph for Vin and Vout on PCA9306, please let me know.
※Example image is attached below;
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Eric-san
Thank you for reply,
I answer your question, please see below;
①About Vref1 and Vref2
Customer condition is "Vref1=1.8V±%2.5" and "Vref2=3.3V±%2.5"
②Pull up resistor
Both side are 560Ω±%1
③Background for this plot
Customer want to check Vin/Vout spec for between Master and Slave.
If you find the point of better to change, please change this point. (For example, pull up resistor value, etc)
Best regards,
Satoshi
Satoshi-san,
Apologies for the delay, I found a PCB to test this on today. Is there any way you can send me the test setup used for these measurements? I want to verify I have the exact setup so I can get the same plots. Maybe a quick block diagram, nothing too detailed. If not, answering the questions below would help.
Regards,