Hi Team,
Would you let me know full sequence of I2C Write/Read with TCA9548A?
SYSTEM Configuraiton.
TCA9548A(Slave address 0x70)
8 I2C device(Slave address 0x10~17, Data address 0x01~0A)
Q1. Write to Ch7 device addres 0x09 value to 0x01
0xE0(TCA9548A slave address 0x70 and write bit) => 0x80(enable CH7)
0x2E(select I2C device, 0x17 which connect to CH7 with write bit) => 0x09(Data address) => 0x01(Value)
Q2. Read from CH7 0x09
0xE1(TCA9548A slave address 0x70 and read bit) => 0x80(enable CH7)
0x2F(select I2C device, 0x17 which connect to CH7 with read bit) => 0x09(Data address which that want to read) => wait
Thank you.
Best Regards,
Jade