Hello,
In my customer using, the LVTTL device is connected at the SDA2 side and Open Drain device is connected at the SDA1 side.
LVTTL device VOH(min) is 2.4V and VOL(max) is 0.4V.
They are considering Figure 7 connection.
I have some questions in this conditions.
(1)
Can we use this device with this condition?
(2)
If the SDA2 input is High, the internal switch is off?
From the following post, is the internal switch always ON when the EN input is high?
https://e2e.ti.com/support/interface/i2c/f/390/p/566841/2083016#2083016
I think that we couldn't level shift if the switch is always ON.
Could you please let me know the SW turned on/off threshold voltage at SDA1/SDA2/SCL1/SCL2?
I think that it depend on EN voltage but I couldn't found the information.
(3)
If the SDA1 side is high(I2C device open drain output), is the internal SW of PCA9306 turned off?
Best Regards,
Ryuji